STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32 STOP mode with LCD

In an aplication using STM32L0 I need to enter the STOP mode when I realize the AC mains disappears and the uC must be powered by a battery.So before entering the STOP I obvioulsy deinit all the peripherals used till then and put the pins in analog m...

MVill.6 by Associate II
  • 2943 Views
  • 4 replies
  • 0 kudos

Touchgfx stops after enabling interrupt

So I have a gui runing on touchgfx part, i want to sample adc using interrupt mode but when ever i run adc in continuous mode the screen blanks out.Similar thing while enabling timer interrupt But for the timer if the interrupt in like greater then 7...

JLoda.1 by Associate
  • 1325 Views
  • 1 replies
  • 0 kudos

LTDC color issue

Hi,I am faced with some color issues on a custom board (STM32H7A3). A 800x480 24 bit LCD is connected and the LTDC pixel format is RGB888. For testing is set the background color within LTDC initialisation to:  hltdc.Init.Backcolor.Blue = 128; hltdc....

0693W00000QKwntQAD.jpg
SSchw.7 by Associate
  • 2433 Views
  • 2 replies
  • 0 kudos

Resolved! External loader fails to download

Hi all,I'm trying to put some TouchGFX data (images, text, ...) in an external flash (S25FL128L) on a custom board with STM32H7B0VB mcu. I'm using the octo-spi peripheral as quad-spi.So, I followed the guide to make an external loader and I did it. I...

nikof by Associate II
  • 10010 Views
  • 15 replies
  • 0 kudos

TouchGFX 4.20 containers code error

Error[Pe738]: a class-qualified name is required E:\project\insulation\iso_monitor\isoMainx\TouchGFX\generated\gui_generated\include\gui_generated\containers\CCDisResDiagBase.hpp 33  touchgfx::GraphElementLine ;Error[Pe029]: expected an expression E:...

sxiao.1 by Associate II
  • 1170 Views
  • 1 replies
  • 0 kudos