STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I have a problem in my TFT LCD project. I use LTDC, FMC, SDIO, and Touchgfx. I read all of the images in stm32f429 from the SD card. some of the images in my project don't load correctly. what should I do? and what is the reason?

as shown in this picture (the top picture is in Touchgfx and the bottom picture is in my LCD board) some images in my LCD don't load correctly!my code :void StartDefaultTask(void const * argument)   {   /* USER CODE BEGIN 5 */     f_mount(&SDFa...

0693W00000Subh1QAB.jpg

Unable to locate .ioc Path error from TouchGFX tool

I got one error:////////////////////////////////////////////Post Generate Target    touchgfx update_project --project-file=../VHD_V1_Released.ioc --platform=m7    Unable to locate C:/Users/Pratik.JPanchal/Documents/STM32CUBE_IDE/workspace/VHD_FINAL_P...

PPanc.1 by Associate II
  • 2855 Views
  • 3 replies
  • 0 kudos

Long Press Button Using Hardware push Button

Hi,I am designing counter with hardware button using Nucleo-F767ZI (freertos) with GFX01M1. the idea is when i hold the push button (eg. 5 sec or more) counter will increase by 10 each if single press, counter will increase by 1. right now it's only ...

SZY.1 by Associate
  • 2063 Views
  • 2 replies
  • 0 kudos

mvp concept at custom container level

I have designed my small component as a custom wedget that will be embeded in many screens. This component need do some data interations with background system.As document suggested, I would like to use MVP architecture to implement data exchanges. B...

shark by Senior
  • 1810 Views
  • 4 replies
  • 0 kudos

Change Wildcard text fore color on a FlexButton

Created this function where want to pass a flex button as a parameter to the function and change it's text color.Changing the text color directly using the object name works, but when I pass the button to the function I cannot get it workAny help ver...

0693W00000Uo6UgQAJ.png

Resolved! Pressed button image

Hello,Is it possible to use bigger pressed button image than released button image? How can I achieve it?

0693W00000UnwIaQAJ.png
heyo by Senior
  • 4094 Views
  • 15 replies
  • 0 kudos

Reduce code size for bootloader

We currently have a bootloader we have been using in our products. However it was created with emWin and we are transitioning everything to TouchGFX. The current boot loader fits in code space of 0xC000 and includes a few text updates to the 480x27...

RLarr.1 by Associate III
  • 2202 Views
  • 3 replies
  • 0 kudos