User Activity

hello​I want to know if it is possible to implement the attached gif image function with the "Progress" function.​Is it possible to implement with gradient progress?​Or can you show me how to make a gradient image in advance with Image Progress?​​Bel...
hello​​Among the TTF fonts, there are special characters that cannot be directly input from the keyboard. Is there a way to input them in GFX?​For example, #code...​thank.​​
When the external 5V power of the STM32H735g-dk board is supplied, intermittently, the initial reset does not work normally.​STM32H735g-dk​CubeIDE​Downloading the latest version of CubeIDE and CubeProgrammer does not solve the problem.​​If the initia...
hello,​​I am trying to run the project created with TouchGFX in STM32H735D-GK.​It seems that the operation period of void Model::tick() of Medel.cpp is longer than 10ms instead of 10ms.What exactly is the operation cycle of Medel.cpp's void Model::ti...
helloI want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.​An operation has occurred.​used STM32H735G-DK ​/ CubeIDE 08:16:59 : STM32CubeProgrammer API v2.9.0 08:17:02 : ST-LINK SN...
Kudos from