STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to access or reference a variable set in a custom container from the screen containing that container

I have a custom container that pops up on a screen for password entry. The password is set using 4 scroll wheels and an entry button with icon. When the entered password matches the required password a flag variable is set and the custom container is...

UART sending data problem using TOUCHGFX

Hi, Im working on touchgfx with STM32H750XBH-DK eval board and gyro sensor. So I try to display the data using UART which I want to display using serial monitor(tera term) but its doesn't work and nothing display in my monitor.Basically i have try us...

0693W00000Y6tNwQAJ.png
Angle by Associate II
  • 1534 Views
  • 1 replies
  • 0 kudos

LVGL and Square Line Studio for STM32F469i-disco

I need help with using lvgl in stm32f469i-disco. Currently iam using touchgfx for the graphics tft, but i see lvgl has much feature and clean design. is there anyone has experience with lvgl? Please help, any references or source code will help me mu...

BAl K.1 by Associate III
  • 2184 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F429I-DISC1: Is there a simple way to create a touchGFX project that has an .ioc file ?

for STM32F429I-DISC1, the Designer creates a project that does not contain an .ioc file. This means that any functionality additional to the graphics must be configured by code instead of CubeMX. Is there a simple way I can have an .ioc file in the p...

Resolved! STM32CubeIDE: Different File Structure

I am using the STM32H7B3I-EVAL, which includes a touch screen that uses the TouchGFX application. I am trying to do its tutorials, which includes modifying the code in the STM32CubeIDE. However, when I do, the file structure is different in my comput...

0693W00000UnLQNQA3.png 0693W00000UnLQhQAN.png
KMew by Senior III
  • 15831 Views
  • 21 replies
  • 0 kudos

Why does my LCD look like a horror movie?

I've got a strange issue. STM32H757I-EVAL board that is about 3 weeks old. I've been working on a board bring-up for a week and pulling my hair out. So I used an existing project and thinking that maybe I'm not crazy. This is what I see on the LCD ->

0693W00000Y78tiQAB.jpg

snprintfFloat prints incorrectly some numbers

For example Unicode::snprintfFloat 70000.700f with "8.2f" incorrectly prints "70000.71", while snprintfFloat 60000.700 with "8.2f" correctly prints "60000.70"Test code:Unicode::snprintfFloat(textArea1Buffer, TEXTAREA1_SIZE, "%8.2f", 70000.700f);   Un...

Tuoman by Senior II
  • 2430 Views
  • 4 replies
  • 0 kudos

GFX01M2_HelloWorld application on X-Nucleo-GFX01M2 w/ STM32G071 Nucleo. IAR makes, I can build, but attempts to download/debug do not work. Basic G071 demos work.

My Debug Log = Thu Dec 29, 2022 14:43:39: IAR Embedded Workbench 9.32.1 (C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm\bin\armPROC.dll) Thu Dec 29, 2022 14:43:39: Loaded macro file: C:\Program Files\IAR Systems\Embedded Workbench 9.1\arm/co...

PFabi.1 by Associate II
  • 4954 Views
  • 7 replies
  • 0 kudos