STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Issue: locked Elements don't stay where they are

After update TouchGFX 4.20.0 to 4.21.0, all fixed element on the screen don't stay where they are meant to be. I post the following image, in which the Text element and MORE-logo element are locked. But after simulation these elements are all arrange...

0693W00000Y7UVJQA3.png
JPan.4 by Associate III
  • 2461 Views
  • 4 replies
  • 0 kudos

Root folder image problem

I am working with touchgfx 4.20.When I have an image in the root folder of the touchgfx I am able to display the image on th e LCD but when I make a folder in root folder and move the image there it runs into a hardfault. Can you please help me with ...

rohan_m by Senior
  • 2867 Views
  • 7 replies
  • 0 kudos

DMA2D HAL_DMA2D_Start -> pdata(color) formar

HelloI got LCD 240x320 connected via SPI to my STM32f429. LCD interface is RGB565.I have created buffer uint8_t buffer[240*320*2]; so, 1st im filling buffer with red color: for (int i=0;i<240*320*2;i+=2){   buffer[i]=0xf8;   buffer[i+1]=0x00;   ...

aadam.1 by Associate
  • 1616 Views
  • 1 replies
  • 0 kudos

LTDC Reset after Stop Mode

HeyWe are trying since a few days to reset our Display after Stop Mode, without much success. We are using a STM32F767IIT6 and a 480x272 Display, which is driven over the LTDC. Our code is appended.When the power button is pressed, we set a flag. We ...

MStud.4 by Associate
  • 1277 Views
  • 0 replies
  • 0 kudos

Debugging with Images in External flash and TouchGFX

I am using controller STM32H745BIT6 device with QSPI flash connected.I have configured the TouchGFX to keep images in external flash and also configured .LD file to create section ExtFlashSection. Am able to see the memory assigned to images in the S...

ATank.1 by Associate III
  • 992 Views
  • 0 replies
  • 0 kudos

TouchGFX 4.19.1 Screen Glitch on STM32H747I-DISCO

Hi,I am working with TouchGFX and an STM32H747I-DISCO. I have created a very simple project comprising two screens.Each screen has a box covering the entire canvas (one set to white and the other to black) plus a single button in the bottom right cor...

Rob H by Associate
  • 2034 Views
  • 2 replies
  • 0 kudos

B-LCD40-DSI1 DSI Data Lane Setting

Hi, I'm working on a project using DSI to print LCD with STM32F769I-Eval.In this kit, there is a display module called B-LCD40-DSI1, and it has a OTM8009A.I build an example called LCD_DSI_CMDmode_SingleBuffer, and it worked.But after I changed numbe...

ELee.9 by Associate II
  • 924 Views
  • 0 replies
  • 0 kudos