STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

why the interface of STM32F769I DISCO KIT generated by TouchGFX is Freezing even for a very simple button test?

to more explainI installed TouchGFX 4.20.0, I developed a simple interface that has two buttons just for a very simple test, I sent this program to the STM32F769I DISCOVERY KIT board, everything goes well, I received the message Run Target DONE, the ...

RMOHA.21 by Associate
  • 1032 Views
  • 1 replies
  • 0 kudos

buttons continuously registering touch events.

I have a touch screen application that I am having issues with. The touch screen works. The issue is that if I press and hold the buttons on my screen the image will toggle between touched/not touched. I am sure I must have something configured in...

PBaie.1 by Associate II
  • 2271 Views
  • 4 replies
  • 0 kudos

Resolved! Interfacing STM32F746G-DISCO with B-CAMS-OMV

Hi ST,Currently I'm working on a project where I would like to use a camera and project the image on the LCD of the discovery board. Now I know that the B-CAMS-OMV should be interfaceable with every STM32 MCU, but I can't seem to get it to work. I tr...

eeeeee by Associate III
  • 3762 Views
  • 4 replies
  • 0 kudos