STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Simulation error: *** missing separator. Stop.

Hello,i know the problem of the error "*** missing separator. Stop." from the build, but i do not understand why it happen here. What i know is that it should have Tab instead of spaces, but line 4 does not have multiple spaces.I created a simple sim...

Multiplexed OctoSPI with LCD 800x480 on STM32H7A3

We are planning a new project and would like to know if the following configuration would work: SMT32H7A3 CPU (280 MHz)Multiplexted HyperRAM and HyperFlash via OctoSPI2 LCD module (LTDC) 800x480 with TouchTouchGFX Graphical user interfaceHas anyone e...

GS1 by Senior III
  • 2390 Views
  • 4 replies
  • 0 kudos

STemwin background color of a text

Hi thereI'm currently working on a simple project and it is a simple 7inch LCD using a STM32H743IIT6 board.I used GUIDRV_LIN for display driver. and I have set all the LTDC and FMC, etc. here are my issues:1- first: in a simple window I have some TEX...

Ala by Senior
  • 926 Views
  • 0 replies
  • 0 kudos

I'm trying to get a TFT display to work using Touch GFX on a custom board. Why doesn't the display I make in touch GFX show up?

320x240 Parallel RGB (LTDC) interface. I've been following the TouchGFX board bring up instructions. I can change the background color, so the hardware side should be good.I made a display in TouchGFX, everything compiles. TouchGFX updated the files ...

0693W00000Y9ypSQAR.png 0693W00000Y9yqGQAR.png 0693W00000Y9yquQAB.png 0693W00000Y9yrdQAB.png
SWood.4 by Associate III
  • 4370 Views
  • 9 replies
  • 0 kudos

Resolved! LTDC: Display Compatibility Question

Hello,I am looking to use the LTDC (LCD-TFT) feature to interface with a TFT display and potential touch controllers (CTP). I am uncertain on the requirements to interface with it and wanted to confirm a few details.I have written software (generated...

KMew by Senior III
  • 3157 Views
  • 4 replies
  • 0 kudos