STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Slide transition not working with single framebuffer

Hello,I’m trying to understand some issues we have with the slide transition. The slide transition uses the snapshot widget functions to copy the "old" screen to the animation storage to combine this screen with the incoming screen.Here is the code:S...

0693W00000Y9ErIQAV.png 0693W00000Y9EnbQAF.jpg
Pirol by Associate III
  • 1637 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX Designer Default Canvas Buffer Size 0

In TouchGFX 4.20 designer my pages mostly have default 7200 canvas buffer size but some pages default canvas buffer size seems 0 like below;If I do not add a canvas size to these pages manually, this causes errors. Why does this happen on some pages ...

0693W00000YAfsWQAT.png
afergan by Associate II
  • 2613 Views
  • 3 replies
  • 0 kudos

Hi Everyone, I'm total rooki, I just start in stm32 an TouchGFX when I push my "buttonWithIcon1" I need reset on my pin PD6 and otherwise see myscreen2View.cpp for example:

void Screen2View::up1(){   if (buttonWithIcon1.getPressedState()==true) HAL_GPIO_WritePin(GPIOD, GPIO_PIN_6,GPIO_PIN_RESET);   else HAL_GPIO_WritePin(GPIOD, GPIO_PIN_6,GPIO_PIN_SET);}what is wrong, thans for help

LKlen.1 by Associate
  • 2056 Views
  • 4 replies
  • 0 kudos

Resolved! Images on external flash (QUADSPI) mapped in memory and on SDCARD (simultaneously). It's possible?

Hello everyone.I have a custom board based on micro STM32F469NIH6I am using TouchGfx successfully and have all my images stored in a memory mapped 64MB QUADSPI.I would like to give the user the possibility to change some images (for example a logo) a...

DDi S.1 by Associate III
  • 2198 Views
  • 2 replies
  • 0 kudos

Simulation error: *** missing separator. Stop.

Hello,i know the problem of the error "*** missing separator. Stop." from the build, but i do not understand why it happen here. What i know is that it should have Tab instead of spaces, but line 4 does not have multiple spaces.I created a simple sim...

Multiplexed OctoSPI with LCD 800x480 on STM32H7A3

We are planning a new project and would like to know if the following configuration would work: SMT32H7A3 CPU (280 MHz)Multiplexted HyperRAM and HyperFlash via OctoSPI2 LCD module (LTDC) 800x480 with TouchTouchGFX Graphical user interfaceHas anyone e...

GS1 by Senior III
  • 2352 Views
  • 4 replies
  • 0 kudos