STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

touchgfx and usb msc

hello, I need to use both touchgfx and usb msc host with stm32h743 in my project. they work fine separately , but when I add usb to my touchgfx project it does not work(all my usb implementations are based on controllerstech video). Do I need to do a...

Zakba.1 by Senior
  • 2014 Views
  • 5 replies
  • 0 kudos

Resolved! Multi-level menu

Hi all,I would like some ideas/help with designing an interface for a large multi-level menu. I need the user to be able to get to specific information about a vehicle make, model and year. My first thought was to use a scroll list or wheel for the u...

SGill.3 by Associate II
  • 3688 Views
  • 4 replies
  • 3 kudos

Resolved! boxProgress orientation, and circleProgress size

Hi, In my UI project I need a vertucal boxProgress while all available backgrouds and images are horizontal while w&h are greyed out. When I create a custom background, the progress bar is not working. Same for circleProgress (size control). Can you ...

ksale.1 by Senior II
  • 564 Views
  • 1 replies
  • 0 kudos

Resolved! Couldn't reserve space for cygwin's heap

Hi,using TouchGFX, I get the following error when I run the code.How can I fix this?Thanks***************************************************************Compiling simulator/main.cppCompiling touchgfx/framework/source/platform/driver/touch/SDL2TouchCo...

AndreaTW by Associate II
  • 531 Views
  • 1 replies
  • 0 kudos

Resolved! Font not discovered in ./assets/fonts

Hi,Using Designer 4.25, I copied a font to ./assets/fonts folder but it is not in the list"Solido Compressed W00 Bold.ttf"Name displayed by OS is "Solido Compressed W00 Bold" when open in FontForge Any idea how to make the Designer to recognise the f...

ferro_0-1743415790407.png ferro_1-1743415823191.png
ferro by Lead
  • 996 Views
  • 3 replies
  • 3 kudos

Resolved! TouchGFX for custom display

HI,I´ve to design a solution with a custom 5 and 7 inch color displays for a more or less static graphics (just some values and maybe some charts).Which interface / MCU would you recommend? MIPI-DSI? Would be fine to have a quite small MCU (preferrab...

AWack by Senior
  • 694 Views
  • 4 replies
  • 0 kudos