cancel
Showing results for 
Search instead for 
Did you mean: 

[Potential Bug introduced in v4.25] Calling virtual method in AbstractPainterColor constructor

millerjeremy
Associate

Our team updated a project from v4.22 to v4.25 this week and our clang-tidy scan flagged the following warning message in the constructor of every class that had a "Painter" member variable ("Painter" is aliased in our solution as "using Painter = touchgfx::PainterRGB565;").

 

AbstractPainterColor.hpp (External\Middlewares\ST\touchgfx\framework\touchgfx\widgets\canvas)

Call to virtual method `AbstractPainterColor::setColor` during construction bypasses virtual dispatch [clang-analyzer-optin.cplusplus.VirtualCall, -warnings-as-errorss] GCC [Ln45, Col9]

Container.cpp[Ln 29, Col12]: Calling default constructor for 'PainterRGB565'

PainterRGB565.hpp[Ln 43, Col 36]: Calling default constructor for 'AbstractPainterColor'

AbstractPainterColor.hpp[Ln 45, Col 9]: Call to virtual method 'AbstractPainterColor::setColor' during construction bypasses virtual dispatch

In looking at the warning message, it's not necessarily a problem, depending on the intent.  

Depending on the intent, it appears this is fine, but here's some noteables:

  • AbstractPainterColor's constructor changed from explicitly calling AbstractPainterColor::setColor(...) to simply setColor(...). (introducing the warning)
  • PainterRGB565 also defines a setColor(...) method (and inherits AbstractPainterColor).
  • As long as there is not a presumption that AbstractPainterColor's constructor is calling PainterRGB565::setColor(...), I think it is fine to suppress the warning, which we are doing.
  • If for some reason that is incorrect, either we have a misunderstanding on how things work or the behavior is not as was desired with this change (or perhaps is undefined) due to the fact that "the more-derived class does not yet exist" per cppreference.com.

Perhaps this is fine (and/or my understanding of the message is incorrect), but it might warrant a closer look by the TouchGFX development team if the actual behavior is not the desired behavior in this case.

1 REPLY 1
Maxime_MARCHETTO
ST Employee

Hello @millerjeremy,

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

Best regards,

Maxime


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.