STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32G0 board with custom LCD with 1bpp

Target Board: STM32G0  LCD Used: UC1629 256*160  No RTOSI am using scroll list widget to display my menus and have switches to navigate between screens. When I put 2 as the no of items on the screen, the scroll list is working fine, for 3 only part o...

why so difficult to use and code with touchgfx ??

Hi Guysbeen use to developing C and embedded ST nucleo boards, now venturing in to touch gfx, must say seems very convoluted and hard work and very timely! using touch gfx seems so long winded to do simple tasks with graphics ??i'm using the designer...

JHERI by Senior
  • 1483 Views
  • 1 replies
  • 0 kudos

Resolved! Honest opinion required: STemWin vs TouchGFX

I have to work on a long term project that involves using the LCD on the STM32H745XIH6 board and deciding which pathway to choose is crucial at the beginning of a project to avoid as much hassle as possible.If I use STemWin, will I get support from t...

How to change screen transition heap ?

Hi ,I've implemented multiple screen in my project(Custom project using STM32F429zi controller with external RAM and Flash). I'm getting memory fault issue whenever I'm transitioning from one particular screen to any other screen. When I debugged I g...

tuka214 by Associate
  • 1392 Views
  • 1 replies
  • 0 kudos

Resolved! FUTURE REQUEST For Touch GFX, please ARRAY! ARRAY! ARRAY!

HelloI'm still very new to Touch GFXStill finding my way with programming in C++ as I'm more C based,The biggest drawback I’m finding is the TouchGFX design environment when laying out screens does not allow you to add objects (Widgets) as arrays (mu...

JHERI by Senior
  • 7446 Views
  • 15 replies
  • 1 kudos

Swipe Container Detecting Swipe

Is there a way of detecting a swipe has been performed using the swipe container?I see others have used some callbacks but these posts are a few years old.I would think this would be a "default" out of the box functionality, after all it is a SWIPE c...