STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Button with svg image?

Hello everyoneCan I also add an svg image to a button? I can embed images in svg format (almost) without any problems. However, if I want to assign an image to a flex button, only png works. Is there a workaround for this or does it just not work?Reg...

Roger.ch by Associate III
  • 3268 Views
  • 1 replies
  • 2 kudos

Libjpeg-Turbo on STM32F4xx?

I'm currently working on a project that needs to decode JPEG's and do so as fast as possible, natuarlly I've looked for alternatives to the libjpeg offered by CubeMX and stumbled upon Libjpeg Turbo which uses SIMD instructions to optimize the de-/com...

KK.2 by Associate III
  • 2039 Views
  • 1 replies
  • 0 kudos