STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

[STM32L496G-DISC0] Project generated from Touch GFX Designer not compileable in CubeIDE (undefined reference to 'LCD_IO_***')

I'm trying to build a Touch Application using the STML496G-DISC0 Board. I try to create my project using the TouchGFX Designer App, selecting my Board and either a blank or the one matching Template (doesn't make a difference in this case). I can tha...

0693W00000BZfYDQA1.png
Janek1 by Associate II
  • 2690 Views
  • 5 replies
  • 0 kudos

multi touch controller ILI2511 USB interface

I am having 10.1 Inch display with CTP. The touch controller is ILI2511 at USB interface only. It is configured as multi touch point touch pad.I connected touch panel with PC, it is detected by PC and multi touch test screen appears on PC screen, whe...

Resolved! New STM32H747-DISCO example problems.

Hi There,I have a new STM32H747-DISCO here.The board came without the demo flashed on it, also the demo can not be flashed, see here: https://community.st.com/s/question/0D53W00002ASl3lSAD/stm32h747-discovery-blankMost of the examples in the cube pac...

ACapo.1 by Senior
  • 11350 Views
  • 16 replies
  • 0 kudos

Using CubeIDE 1.2.1 on Windows 10, TouchGFXDesigner's generated code doesn't implement virtual method HAL::taskEntry() in TouchGFXGeneratedHAL or ToughGFXHAL..

I've generated a STM32F429I-DISCO project using CubeIDE's CubeMX.I've added the X-CUBE-TOUCHGFX 4.13.0 software to the project, under Additional Software.By changing LTDC and FMC settings, I was able to configure X-CUBE-TOUCHGFX successfully.The proj...

CDew.1 by Associate III
  • 2004 Views
  • 2 replies
  • 2 kudos

Resolved! TouchGFX: Scalable Image Memory Allocation Calculation

Hello,I am trying to optimize a TouchGFX project to see if I can fit it all in a 1 MB internal flash (stm32h725agi6).The design our graphic designers have come up with are requiring the same image, but two different sizes. This leaves two options:1) ...

KMew by Senior III
  • 2105 Views
  • 2 replies
  • 0 kudos

Translation sheet on 4.22.1 TouchGFX version

 Hello,In previous versions of touchGFX, I could easily translate texts by editing an .xlsx file and then replacing it in the assets folder.However, I've noticed that in version 4.22.1, there is only an .xml file generated when I create touchGFX file...

GMene.785 by Associate II
  • 2320 Views
  • 2 replies
  • 2 kudos

Aligned to center text comes out cut

Hi,I was placing text into a text area, and no matter what I do, it comes out cut from the sides.the code:  textArea1.setTypedText(touchgfx::TypedText(T_ID_PLACE_CART_IN_CARTON));invalidate(); the result:I suppose it could be the bounding area, but h...

ArthurStone_0-1699966713230.png