STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Busy indicator implementation

Hi All,I'm trying to implement a busy indicator.I have a set of 24 images generated as frames from .gif file.I used couple of techniques.First one being texture mapper to rotate a single .png  and the smoothness of the busy indicator rotation is not ...

KNara2_0-1702448639227.png
KNara.2 by Associate III
  • 2136 Views
  • 3 replies
  • 0 kudos

Is it possible to overlay things created by C++ code, i.e. Circular Progress Bar, with things from graphical editor?

Hello,working with TGFX 4.10. I use the circular progress bar from git, respectively from one of the examples and so far I'm happy with it although it's a bit strange not to have it in graphical editor...Now I need to overlay it with additional butto...

0690X00000AreuKQAR.png

io ports not controlling

sir we are using the stm32f7508-dk board , code is generated  through touchgfx working properly (display part). when add led toggle code , led not toggling ,

kishor by Associate II
  • 1392 Views
  • 1 replies
  • 1 kudos

Resolved! Unknown interrupt on EXTI2 with GUI STemWin

Hello!Im having some problems with STM32F429ZIT about the interrupt handler. My microcontroller is connected on a LCD display by LTCD bus pheripheral and also has a interrupt input pin (PG2 - EXTI2 on falling edge detection border) connected on a ext...

TiagoAQ by Associate
  • 5232 Views
  • 3 replies
  • 0 kudos

TouchGFX 4.22.0 Designer bug with flex button actions

I got a project with a flex button in screen and custom container with the same name ("ButtonBack"). Both flex buttons got an action to call a virtual function. After generate, close TouchGFX Designer and reopen, the reference button in action is mis...

FDigi by Associate III
  • 1814 Views
  • 1 replies
  • 1 kudos

Scrollist without scrollable conatainer

Hey I have 5000 data that i want to display it in scroll list , means total index of scroll list is 5000so How can i manage it in scrollable containers. I have tried after some data(1000) its not supported please let me know solution

APate.18 by Associate III
  • 2106 Views
  • 3 replies
  • 1 kudos