I installed touch 4.10select STM32429I-Disc1after combining package:1 At startup and when I pressed "Run Target" or "Generate Code" the program shows: "Error during code generation".2 When I pressed "Run Simulator": "Unable to lounch simulator".W...
My TouchGFX works on other PCs (on a virtual machine and at home), a problem with a working PC, administrators cannot helpI compared, all the same on all PC
On Windows 7 Pro 64-bit SP1 don't work!!! (at work).Administrators could not do anything.Tried to reinstall but the result is the same.There were no difficulties.On Virtual Machine 32-bit all Ok (at work)On Windows 10 64-bit all Ok (at home).