STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX analog clock glitch, arms rotating counter clockwise 360 degrees, when passing midnight

I've found a bug in the analog clock widget. It works perfectly, except when passing midnight, then the arms go all over the place. I think they go in the wrong direction first and then bounce a few times. I've attached a video and an example project...

Resolved! TouchGFX Performance

Something I've seen (with all embedded GUI software) is the need for more speed and support for more art asset types. I've written my own imaging codecs (originally for PC). Recently I created new versions that are optimized to run on constrained tar...

bitbank by Associate II
  • 1579 Views
  • 1 replies
  • 0 kudos

Resolved! rendering time of not-visible objects

Hi,how is supposed to work rendering of objects set as "not visible"? My layout is composed of several containers/objects whose visibility is turned on or off at runtime.I've noticed that rendering time is high also when objects are hidden, as if the...

Resolved! TouchGFX compile problems

Hello, i am unable to compile a touchgfx project.Try #1:Starting from CubeMX, Version 6.10.0 i click on Generate Code. It ends with "The Code is successfully generated under:".  When i click on Src/ApplicationTemplate.touchgfx.part, it opens TouchGFX...

sk-st by Associate III
  • 15665 Views
  • 20 replies
  • 0 kudos

Resolved! What is the cause of the screen shift?

Hi All,Im working with a Custom board using STM32h743 and an RGB Display with ST7796 driver.I'm configuring SPI to send the right settings to the display for working with RGB pins on LTDC.In effect I done the 90% of work but I don't understand the re...

1711660943698.jpg Screenshot 2024-03-26 224658.png
MPast.1 by Senior II
  • 2061 Views
  • 3 replies
  • 0 kudos

Resolved! ST boards and 10" touch screens?

Hello people.First of all... I haven't worked with screen displays before, sorry if this post sounds dumb:Now that I said the above:I want to interact with any ST board GPIO through GUI buttons. I also want to do this on a "big" touch screen with gre...

I have a problem with a Riverdi 10.1 display.

Hello, I hope you are well.The problem is, I create a project in TouchGFX Riverdi_101STM32H7 v2.2.0 (to get the BSP folder), I generate the code in TouchGFX, then I open the STM32CubeIDE, I compile with STM32CubeIDE and I don't have any error. I try ...

FGuti.1 by Associate II
  • 3156 Views
  • 4 replies
  • 1 kudos