Question
TouchGFX 4.22.1 TextKeysAndLanguages.hpp and others are missing
Hi,
i'm using cubemx and updated from touchgfx 4.21.2 to 4.22.1 and also installed the newest touchgfx designer.
After regeneration of the project certain files like TextKeysAndLanguages.hpp are missing. So all my texts are missing.
i can see it in my git that these files were deleted

Also <fonts/ApplicationFontProvider.hpp> is missing and generates build errors
In TouchGFX designer i see all my texts and this is my text config (which i did not change after updating from the last version)

Any idea what might be the error?
Regards