dynamicBitmapCreateExternal() does not work for a RGB565 image
Hi,
So I'm pretty sure I've discovered a bug of varying severity related to having a bitmap image in memory and trying to add it to TouchGFX with the dynamicBitmapCreateExternal() function.
I found this in our project board using a STM32H750 with 480x800 display using 16-bit colour depth. But something similar/also wrong appears to occur in the Simulator (using 4.20.0) and on a STM32F429 Disco board.
I've narrowed the scenario down to the following, having tried to isolate all our code from the problem.
- Create a new project with empty screen. Add one image to the screen, but with no image selected.
- In the user code (sub-class) for the view, add some code to generate or otherwise use a bitmap image of RGB565 format. You can use a predefined one, or just generate an array of pixels to use (using touchgfx::LCD16bpp::getNativeColorFromRGB(255, 255, 255) or similar for each 16-bit pixel).
- Create a BMP cache using Bitmap::setCache(), and then register the bitmap using dynamicBitmapCreateExternal().
- Set the image widget to use the registered bitmap with dynamicBitmapCreateExternal().
When drawing, various things will go wrong.
- On our board where I can debug, I get a hard fault with a stack trace showing a call to touchgfx::LCD16bpp::blitCopyAlphaPerPixel() from touchgfx::LCD16bpp::drawPartialBitmap(). The disassembly is dereferencing an address outside of memory space (0x10040). But this only seems to crash when the dimensions of the image cause overflow of 16-bit numbers (> 65535).
- On the F429 Disco, there is no crash. But generating a single colour bitmap of white/black/grey results in a background of various pixel colours - like a corrupted jpeg or something - not a sinle colour.
- On the simulator version of the F429 project, the simulator crashes when trying to draw the screen. GDB will not give me any help so I can't see where it is crashing.
For every one of these though if instead I use a dynamic bitmap of ARGB8888 format, it always appears with no problem and exactly as I created it, e.g. solid grey or white etc.
I think there's a bug in the use of the external bitmap in the RGB565 format. There's also no problem if I use an 'embedded' image (i.e. appears in bitmap_database.cpp).
Can anyone assist or confirm if they've seen this work? I've attached a zip of my F429/simulator project for anyone interested enough/STM support to investigate or at least I would have done if zips were allowed.