STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to store the touchgfx image to SD card?

Hi all,I have touchgfx project which has many pictures, so I must store them in the SD card.I follow the touchGFX document and I meet some issue.The document said:We can extract the binary data for the bitmaps from the .elf file with a simple objcopy...

Junde_0-1716516821889.png
Junde by Senior III
  • 1680 Views
  • 1 replies
  • 0 kudos

Resolved! Multiple Custom Container with FlexButton Callbacks

Hi,I have been struggling to get my head around the way custom container call backs work.I have a custom container that has three flex buttons, this container is then used on a single screenview multiple times.I'd like to be able to identify the flex...

Resolved! Nucleo-f767zi and x-nucleo-GFX02zi CubeMX and HelloWorld

Hello, I am new at the STM32 World.  I started to buy a nucleo-f767zi and it worked fine.  I was not able to get the debug Console running. Like other too.  Because of that I bought the extension Board  x-nucleo-GFX02zi which should be working fine w...

Carsten73 by Associate III
  • 6302 Views
  • 15 replies
  • 0 kudos

Resolved! Explanation of data flow in TouchGFX?

Hi Sir, I am new to embedded world and i have a stm32f429i-disco with touchgfx software.Actually i created a project using touchgfx and generated code using that software.But when i am going to change some code in that generated code file, i can't un...

NS.16 by Associate II
  • 4297 Views
  • 6 replies
  • 0 kudos

Resolved! TouchGFX textArea config abnormal

Hi all,When I config the textArea initial value, the character order I config is different with the display order.After some test, I find this is because of the character "-".I already meet this multi-times, is this a bug?Thanks

Junde_1-1715331930788.png
Junde by Senior III
  • 1720 Views
  • 3 replies
  • 0 kudos

Resolved! Error compile simulator

Hello ST community,i hope you can help me with this errorI am developping touchgfx application and i nedd to display water volume in the screen, so i made some changes in my code and i compile with stm32ide i build it , the console show no error when...