User Activity

Hello Everyone,I have 24 bit Display having 800 x 480 resolution.Also,I have fmc interface having stm32h753bit6 microcontroller with nor flash mt28ew128aba1lpc of 16MB and external sdram of 8MB .External SDRAM is working fine with touchgfx as double ...
Hello All,I'm using custom board that has STM32H753BIT6 microcontroller for this i need to integrate Touchgfx that should use cmsis_v2 OS along with LTDC feature.I tried in display 800 x480 that uses LTDC feature, where project code is in baremetal  ...
Hello everyone,I have Custom board that has STM32H7 controller.I wanted to interface display module G070ACE-LH3 and i have RGB to LVDS  DS90C385AMT/NOPB.As I am a beginner wanted using Stm32 LTDC interface to bring up the display.Can anyone help me w...
Kudos given to