User Activity

Hello, I have made a custom external flash loader(.stldr) file for my STM32 based board. Reading the content of the external flash via CubeProgrammer works fine. But when programming i run into the following problem: CubeProgrammer tries to write par...
since i Updated to TouchGFX 4.21.0 (from 4.20.0) the LCD shows a visual artifactit happens when rendering images in the L8_565 format (plain RBG_565 works) or texti'm using a STM32 nucleo board with a STM32H7A3 processorwhen i generated the code with...
Kudos from