STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to load Touchgfx files to external flash

I have W95Q64 flash memory and STM32F429 custom board. I want to load Touhgfx files to external flash memory. For this purpose, firstly I added below declarations into FLASH.id file as;SPIFLASH (r) : ORIGIN = 0x9000000, LENGTH = 8MandExtFlash...

0693W000006Eu2GQAS.png 0693W000006Eu67QAC.png
Btovi.1 by Associate II
  • 4642 Views
  • 6 replies
  • 3 kudos

Touchgfx issues with dual core

I am using STM32h747 MCU, CubeIDE my question: My controller is dual core, So .cproject file is created inside each core folder. So for touchgfx i have to copy .cproject from inside CM7 to outside, otherwise touchgfx is not able to find. Is there any...

k_c2024 by Associate II
  • 1332 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX and RVT121HVLNWC00-B display selection

I am currently experiencing issues with the TouchGFX tool, as there is no option to select the RVT121HVLNWC00-B (STM32H757X) controller. Could you please provide some details regarding the interfacing of this controller with the display? Actually I'm...

sai1 by Associate II
  • 1460 Views
  • 1 replies
  • 0 kudos

Resolved! Ident number of button in custom container

Hello,I got a screen including 4 text areas with wild card and a 4 flex buttons on top. Clicking a flex button trigger a keyboard that allows to change the content of the corresponding text area.When any flex button is clicked, I manage to identify w...

JJame.1 by Associate II
  • 4099 Views
  • 7 replies
  • 1 kudos

Integration of MIPI DSI Display with TouchGFX

Hi,We built a custom board using STM32L4R9AI MCU. The board contains a display with following specificationDisplay driver: RM69330Connection Interface: MIPI DSIDisplay Size: 454x454We can initialize the display properly because the all pixel can be t...

SSG_0-1719567919933.png SSG_1-1719567976275.jpeg
SSG by Associate II
  • 2067 Views
  • 2 replies
  • 0 kudos

TouchGFX hardfault while screen transition

Hello,I am working with STM32F469 DISCO with IAR and TouchGFX and I am getting a hardfault exception when doing a screen transition from one screen to other one.When the screen has few widgets, this hardfault does not occur. When the screen has more ...

MMostafa by Associate II
  • 1419 Views
  • 2 replies
  • 0 kudos