User Activity

Hi,I'm using a custom H7 board, with QSPI + 16-bit SDRAM, and using RTOS.However I run into an issue where there's glitching in my gauge in TouchGFX (see attached video...)TouchGFX is using double buffer, also animationStorage: setFrameBufferStartAdd...
I am currently working on a TouchGFX project with an H7 custom board with QSPI external flash and SDRAM.I am able to get the display working properly when not using the external flash.The external flash has been tested separately by writing to it & u...
Hi, I have a custom board using STM32H7B3 with the MT28EW128ABA1HJS-0SIT NOR Flash, and I'm getting an error trying to initialize the NOR Flash during HAL_NOR_Init.   /* Get the value of the command set */ ... else // 16 Bit { NO...
Kudos given to