STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Keyboard Efficiency

 Hello, I was hoping for some help on which way to use a keyboard on TouchGFX. It will be the same keyboard from the example provided by TouchGFX. My application has multiple screens (10-12) where it uses a keyboard. Would it be more efficient memory...

Priyank by Senior
  • 2726 Views
  • 6 replies
  • 0 kudos

TGFX Designer 4.24.0 Download Problem

I can't download TGFX Designer 4.24.0. I select it from the drop-down list, confirm the license agreement. Instead of downloading the archive redirects to the page. If you select other versions, the archive is downloaded    

zema____0-1730108602518.png
zema___ by Associate II
  • 2503 Views
  • 6 replies
  • 0 kudos

Camera OV7675 JPEG Compression

Posted on August 13, 2015 at 18:42Hi,I'm trying to use an ov7675 0.3Mb with the STM32F4209.The main goal is to stream the data through WiFi, using the module AMW006 from ACK.What I'm wondering is to use a specific IC to do the compression to JPEG or...

roger23 by Associate
  • 1791 Views
  • 2 replies
  • 0 kudos

printing updated strings in a model

hello people..actually i want to display a string..i did in this waychar buff[10]="hello";Unicode::snprintf(buffer,10,"%s",buff);but am not getting anything.....in the prinf the buffer is i had the textarea from touchgfx that buffer am taking here......

prathima by Associate II
  • 6819 Views
  • 16 replies
  • 0 kudos

Resolved! Memory on dev kit vs image size

Hi,looking at this dev kit  https://www.st.com/en/evaluation-tools/32f469idiscovery.html#overviewit comes with a 800x480 pixels display and the QSPI is "only" 128Mbit.Am I correct in saying that (without any compression) it can only store just over 1...

Ricko by Senior III
  • 1805 Views
  • 3 replies
  • 2 kudos

60Hz Static graph rendering

Hi, I'm trying to render a 60Hz waveform using a static or dynamic graph widget. The use-case is to render all 480 points at a 60Hz rate, e.g., a noisy sin wave... My graph is size 240x480 pixels using 480 data points. I'm trying to demo this on 2 Ev...

PJD by Associate II
  • 3063 Views
  • 1 replies
  • 1 kudos