2021-11-11 11:11 PM
Hi,
I'm working with STM32F746G DISCO board. I have 4 different image arrays- img1[65536], img2[65536], img3[65536], img4[65536]. I would like to display this on the screen simultaneously one below the other.
In the below program,
int i=0;
while(i<4)
{
pLayerCfg.WindowY0 = 68*i; // incrementing Y position on screen to display next image
pLayerCfg.FBStartAdress = (uint32_t) &img(i); //&img1, &img2, &img3, &img4
HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 1);
}This displays one image at a time in the incremented Y position. entire screen is reloaded everytime.
I tried with - HAL_LTDC_ConfigLayer_NoReload(&hltdc, &pLayerCfg, 1);
But did not display image unless I call - HAL_LTDC_Reload() function where again only 1 image is displayed.
I'm unable to combine all the image arrays to one since 65536 is the max limit for array size initialization.
Please suggest how to display 4 images at a time on screen one below other. Can we configure this board to have 4 different layers display so that each image can be displayed on different layer?
Regards,
Shruthi
2024-06-10 11:48 PM
We are also facing similar issue. Is there anyway to be able to work on this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.