User Activity

Hello.I would use a static graph to display data. In the handletickevent function, I update the addDataPoint(x data, y data) function for the given page, but nothing appears on the graph, the scale is fine, but no line or change in the x direction ca...
Hello!  My project is almost finished, but I had a little problem. On the dashboard, I can optionally read the speed and coolanz water temperature from the can bus or with sensors (vr sensor, ntc). In the case of the can bus, the display works proper...
Hi everybody!I implemented a keyboard into my project. (I tested the keyboard widget in a separated project, and it worked well).If I use the keyboard in my dashboard project, it make weird things.If i entry a value, i write to the eeprom(M95320). If...
Hi all!  I'm looking for a custom numerical keypad, with negative sign, comma(for float vaues) , clear and enter.How can i create? I found only querty, and numerical without comma and sign. Thank you! 
Hello!I have an ART_PI board with STM32H750XBHX MCU and W25Q64 FLASH IC on it.I want to make my own loader, but it doesn't work as it should.Running until the memcmp cycle, I look at the memory map. But the content is not good. There are values 00000...
Kudos from
Kudos given to