STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Orphaned TouchGFXDesigner processes

Process Explorer is showing a number of TouchGFXDesigner processes as running even though all instances of it have been closed (there are no windows visible).I found this when I tried to delete and folder and that failed with an "in use" message - Re...

CTapp.1 by Senior III
  • 2079 Views
  • 4 replies
  • 4 kudos

Resolved! Feature request: Stadium button

1) Using the definition I found here (Wolfram-Stadium).Would it be possible to add an option in the flex button to change into a flex-Stadium/button?I ask this because I saw multiple implementation of keyboards and most of them instantiate way to man...

Marc_LM by Senior
  • 1427 Views
  • 3 replies
  • 0 kudos

Resolved! can't lower nema buffer pool memory usage

Hi,On using svg's on an U5f9, i try to activate the hardware acceleration but this demands to much free memory of my project. the nema buffer create pool function demands 614K of memory, independent of the MEM_POOL_SIZE or the STENCIL_POOL_SIZE. is t...

Jcoop1_0-1730299991916.png
Jcoop.1 by Associate II
  • 2009 Views
  • 3 replies
  • 1 kudos