STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TouchGFX CONTEST RESULTS: Congratulations!!

Hello community!On March 18, we launched a TouchGFX Contest that had for goal for us to see our community's skills and creativity. This contest ended on May 2.We received several interesting projects, and it is now time to announce the winners! Our h...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Respected Sir/Mam , I cannot able use the keyboard example in the ongoing project of the same screen in STM32H7B3I-EVAL.

Respected Sir/Mam , I cannot able use the keyboard example in the ongoing project of the same screen in STM32H7B3I-EVAL.When I have tried to insert it, it is not visible and having blank code inside it. Although Touch GFX 4.17 version has that facili...

Sanchit1 by Associate III
  • 3106 Views
  • 17 replies
  • 0 kudos

STM32F769I-DISCO demo stuck on start up screen

I am trying to get the demos to work on the disco board, but every time I upload the code the ST logo appears and then it hangs.I upload the hex files via STM32CUBEPROGRAMMER where it successfully uploads but always fails to verify giving me this err...

JTurn.2 by Senior
  • 2618 Views
  • 9 replies
  • 0 kudos

Resolved! TouchGFX 4.20 issue with slide transition

I've recently updated with no major issue my TouchGFX project from 4.18.1 to 4.20.0.The screen behaves like before with one major exception: all the slide transitions have become way slower and laggy now with the new version.When previously with 4.18...

TDele.1 by Associate III
  • 1927 Views
  • 7 replies
  • 0 kudos

ScrollList only snapping Top/Left

Currently I'm designing a UI using TouchGFX and like the ease of use. But there are some limitations:A ScrollList can only snap in the topmost (leftmost in horizontal mode) position, if not circular. I've designed dropdown menus, where due to limited...

0693W00000SvZv8QAF.png 0693W00000SvZvDQAV.png
sndstrm by Associate
  • 876 Views
  • 2 replies
  • 0 kudos

Numkeypad

Im doing numbers keyboard and do not know how to change bitmap position then i press the buttonIm using this struct :

0693W00000UnCt2QAF.png 0693W00000UnCweQAF.png
heyo by Senior
  • 973 Views
  • 6 replies
  • 0 kudos

How to edit text?(keyboard)

I'm making a custom keyboard and want to add some extra functionality. I need to be able to edit the texts (i.e. by marking the place of the text and moving the entire text to the right when writing). Maybe someone has done something similar and can ...

heyo by Senior
  • 1665 Views
  • 6 replies
  • 0 kudos

Resolved! TouchGFX Widget TextArea Alignment

I have set up some TEXTS (On Off). I noticed that there are 2 alignment settings here (see #2 and #3) in the imageWhat does the 2 alignment setting do?Then there is the alignment for the actual widget (#1)Which alignment wins as far as the text being...

Resolved! How can I create a TouchGFX Project with the STM32H7B3I-DK and write usercode with CubeIDE?

I have start with TouchGFX, select the demo board and generate the code. Simulator and download works.But now, when I want open the project with CubeIDE, the first is, the project is completly empty. Then when I start a new project with the existing ...

MMüll.6 by Associate III
  • 2343 Views
  • 11 replies
  • 0 kudos

Resolved! How to solve the Enum in struct build error

Not sure what I am doing wrong here in my header file. I have a struct pump_info which has some enums as properties. I get a build error on all 3 on the enums in the struct. Error'operation_mode' does not name a type'operation_mode' does not name a t...