STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1790 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4938 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9684 Views
  • 5 replies
  • 3 kudos

EVSPIN32F0601S1 not running motor

Hi All,I am trying to get up and running the above hardware. I downloaded the software for the board, and we already use IAR compiler here. After compiling and downloading (via the STLink), the system runs the program just fine.However, I just need t...

Resolved! PID tuning under varying Load in STEVAL ESC001V1

ST Documentation describes how to determine prior gains of Current PI controllers. My doubts are:1. Will these gains work for all load conditions? How to tune them under varying load conditions? What is the documentation/process related to it, please...

Resolved! MediumFreq Register Update Frequency

Hello,in file RegListSTMV2.json I can define custom registers. Most registers have "UpdateFrequency" configured to "MediumFreq".How often is "MediumFreq" polled by Motor Pilot?Is it possible to configure the polling frequency in Motor Pilot?Thanks, 

c_dev05 by Associate III
  • 524 Views
  • 1 replies
  • 0 kudos

easySPIN Firmware

Hello, @Peter BENSCH @Cristiana SCARAMEL @TDK @Amel NASRI I recently came across the easySPIN library for controlling a stepper motor using the L6474 driver. The library provides two board options: STEVAL_PCC009V2 and STM32_VL_Discovery.I am using th...

SannanAli by Associate II
  • 1151 Views
  • 1 replies
  • 0 kudos

Resolved! How to configure the motor open loop mode?

hello everybody:    l'm currently debugging the FOC motor with MC Workbench. Now I have generate the code with the open loop configuration. According to the user mannual, I can use the APIs in the code as follows:------------------------------------F...

DF_MC by Associate III
  • 913 Views
  • 3 replies
  • 0 kudos

How run motor using PWM in STSPIN32F0A

I have a STSPIN32F0A board on which, I need support on below points1) Ability to operate the motor through LIN/PWM signal rather than an ADC signal, currently the EVAL board supports an ADC through an onboard potentiometer which I want to remove. 2) ...

HSing.5 by Associate II
  • 818 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.