STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1716 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9546 Views
  • 5 replies
  • 3 kudos

Resolved! Regarding STS pin SPIN32F0A

Hi team,I had made project on Motor control workbench in 5.4.8 where i get serial communication to check the parameter.if i work on 5.Y.4 where serial port is not active, then how to activate the serial port in 5.Y.4?if i import the 5.4.8 project in ...

STEVAL-CTM010V1 PFC enable

Hi, I got a Steval-ctm010v1 board and using sdk 5.4.8. I have tried to enable its PFC section with eliminating the warning from xml file at the sdk file location. It enabled the PFC in the motor workbench and it shows that pins are assigned at the mo...

Resolved! Max modulation control

Hi,It is not an issue with ST software but wanted to clarify, my application requires different modes with speed limitation in each mode, to do that i have started controlling the CircleLimitationM1.MaxModule parameter in torque control mode which is...

STuser2 by Senior III
  • 606 Views
  • 1 replies
  • 0 kudos

DACs not working on EVLSERVO1

Hello,I am using the EVLSERVO1 board and trying to monitor the DAC outputs with an oscilloscope, since the high-frequency plots in Motor Pilot are difficult to use effectively. I enabled DAC Debug in the FOC Wizard, assigning DAC Out 1 to PA4 and DAC...

Isaac1 by Associate II
  • 633 Views
  • 3 replies
  • 0 kudos

Resolved! How to reverse motor direction

Hi All,I have an STM32f302R8 with IHM07M1 with a Bull Runner 2804 motor. This may seem like a simple question but I cannot find any information as to reversing the direction of the motor. In my final project I will need to reverse the direction of th...

DonCorr by Associate II
  • 7471 Views
  • 9 replies
  • 3 kudos