Hello,I have successfully integrated the Bull Running Motor BR2804-1700kv with MCSDK(using the api whichever given by motor control library).But Now, I have to run the motor with raw programming in stm32cubeide. I am using STM32F302R8 microcontrolle...
Hi,I am new to this community. I want suggestion regarding, going to do the setup of two-axis gimbal with Nucleo stm32f429zi and two gdm4108 motors. Is this setup will work?What are all things to cover?Regards,Kamalesh
Hello Gael,I want to design a 2-axis gimbal setup. I have selected GM4108-120T motor. For this motor, IHM07 is the suitable expansion board or Is there driver board will control this motor?Without using mcsdk, we can't program with this expansion boa...
Hello liaifat85,Thanks for your advice. I have selected GDM4108-120T Brushless DC motor.Actually i have chosen the driver board from stm32, which is IHM07M1. It is compatible with the board and if i have to make two -axis gimbal means, how may be the...