User Activity

Does anybody know if control board NUCLEO-F446ZE and power board X-NUCLEO-IHM07M1 can be configured to support 2 motors (FOC) in STM32 MC Workbench? 
I am using MotorControl Workbench (6.2.0) to setup BLDC position control, where Quadrature Encoder is enabled with PPR = 4096. After generating the project, TIM2 is automatically set as Encoder Mode as follows:Now I want to double the resolution with...
I set up a BLDC position control with NUCLEO-F446ZE and X-NUCLEO-IHM07M1. The BLDC motor has integrated rotary encoder, which is connected to X-NUCLEO-IHM07M1. To verify the accuracy of the integrated encoder, I set up an extra optical encoder, which...
I encountered a weird problem when configuring user USB (CN13) of NUCLEO-F446ZE as a virtual COM port. If no other board (e.g., NUCLEO-IHM07M1) is stocked on, this USB can be recognized as a COM port in Windows 10. However, once NUCLEO-IHM07M1 is mou...