2025-01-07 1:54 AM
Hello Everybody,
MCSDK:6.3.0
CubeMX: 6.3.0
Workbench : 6.3.0
Motor Pilot : 1.2.9
I am running on a IHM08M1 with STM32G431, The control is FOC Observer+PLL(sensorless) with 3 shunt.
I want to test the open-loop function of FOC. I have already checked the "open loop" option under "Debug Settings" in the "Drive Settings" page of Workbench. However, when I run Motor Pilot, the "Open Loop - Voltage" control option does not appear in the control menu. Is there anything else I need to configure??
Solved! Go to Solution.
2025-01-07 9:29 AM
Hello @Vincent7,
According to the motor pilot interface, your project has been generated in "profiler" mode. Disable it and generate the project, "Open Loop: Enable" should appear in motor pilot interface.
2025-01-07 9:29 AM
Hello @Vincent7,
According to the motor pilot interface, your project has been generated in "profiler" mode. Disable it and generate the project, "Open Loop: Enable" should appear in motor pilot interface.
2025-01-07 5:16 PM
Hello GMA,
Thank you so mucn, the Open Loop-Voltage option has appeared.