STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4872 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9558 Views
  • 5 replies
  • 3 kudos

STEVAL-SPIN3202, Over current and set SPEED REF

Step 1I have a motorUse EVB-F302+iHM08M1 to get motor parameters through Motor profiler as follows. Step 2I need to use EVB-STEVAL-SPIN3202 of STSPIN32F0A,execute Six-Step Sensorless Example code,STEVAL-SPIN3202\Demonstration\6S_STEVAL3202_SL_VM.stmc...

0693W00000JPevwQAD.png 0693W00000JPevhQAD.png

Resolved! STSPIN32F0 gate driver HS open by default

I'm trying to adapt a piece of BLDC control firmware that already works for the STM32F0 family for use with an STSPIN32F0 chip using a STEVAL-SPIN3201 board. But for some weird reason, I am unable to figure out what's going on with the gate driver, a...

neoxic by Associate II
  • 1396 Views
  • 1 replies
  • 0 kudos

Perform high speed rotation on EVALKIT-ROBOT-1

Hi,I try to perform high speed rotation on EVALKIT-ROBOT-1, my target rotation speed is 6000rpm without loading.I downloaded the example firmware "STSW-ROBOT-1", change values of "DEFAULT_TARGET_SPEED_RPM" and "MAX_APPLICATION_SPEED_RPM" from 4550 to...

ss.3 by Associate
  • 1028 Views
  • 0 replies
  • 1 kudos

ST Motor Control Workbench Stuck at project generation

Hi there!I am trying to spin a motor with a STM32F3 MCU and the Motor Control SDK.I am able to use the Motor Profiler to generate a profile of my PMSM and spin the motor via the computer. Importing the motor profile into the ST Motor Control Workbenc...

krbmr by Associate II
  • 10705 Views
  • 15 replies
  • 1 kudos

Hi, in the Power Stage-Driving Signals Polarity tab in Workbanch. I enabled Complemented from high Side and set HW inserted dead time but I don't know where this is reflected in the program.

当此模�?打开时,计时器的死区时间设置为零DTTest 零�?能直接在 SVPWM 中�?�入死区时间;所以我没有找到一个程�?用于在这�?模�?下�?�入死区时间。如果您能帮助我,我将�?胜感激

0693W00000JOiVHQA1.png 0693W00000JOiVRQA1.png 0693W00000JOiVbQAL.png 0693W00000JOiVgQAL.png
华冠.1 by Associate II
  • 905 Views
  • 0 replies
  • 0 kudos

Causes of Overcurrent Faults (STEVAL SPIN3201)

Hello,I am trying to get the STEVAL SPIN3201 to work with my motor but when the board draws at around 1.1A it always reports an overcurrent fault. I tried to change the motor parameters to see if these are the reason but it had no effect at all. Afte...

MEmmo.1 by Associate II
  • 4407 Views
  • 7 replies
  • 0 kudos