STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1738 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4887 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9583 Views
  • 5 replies
  • 3 kudos

Causes of Overcurrent Faults (STEVAL SPIN3201)

Hello,I am trying to get the STEVAL SPIN3201 to work with my motor but when the board draws at around 1.1A it always reports an overcurrent fault. I tried to change the motor parameters to see if these are the reason but it had no effect at all. Afte...

MEmmo.1 by Associate II
  • 4421 Views
  • 7 replies
  • 0 kudos

Resolved! EVSPIN32G4 current sensing network

Going over the documentation for the EVSPIN32G4, this is the schematics for current sensing:But starting a project in Motor Control Workbench for this board, seems to have different values for the same schematics:Am I missing something? Why the discr...

0693W00000JO2inQAD.jpg 0693W00000JO2iTQAT.png
PCama.1 by Associate III
  • 1306 Views
  • 1 replies
  • 0 kudos

Resolved! Hot to use EVSPIN32G4 on board potentiometer?

Hi all,I'm new to the STM32 MCU familiy, so I've got trouble already doing basic stuff like reading the analog input value of the potentiometer. My main problem is, that I don't understand how multiple measurements can be made on one single ADC. I've...

I am using MCSDK5.Y.2's electric output library. How can I change the current parameters of the motor by directly modifying the source code?

我用的是MCSDK5.Y.2的电出库,�?如何通过直接修改�?代�?,改�?�电机的电�?�?�数?(�?用�?新�?用STM32Cube�?次生�?)我修改了M1_ApplicationConfig_reg.maxMotorCurrent的值,但是�?�有界�?�显示�?�化,实际电�?并没有�?�化。我修改了M1_MotorConfig_reg.maxCurrent值,什么没有�?�化。

ZXuey.1 by Associate II
  • 1068 Views
  • 1 replies
  • 0 kudos

How to start with 3-Phase BLDC motor:

Hi,I have to make low cost on BLDC for Industrial Sewing Machine with Three Hall Sensors and read about BLDC from resources available on internet . I have P-NUCLEO-IHM001 for BLDC motor controland seen below youtube video from ST.https://www.youtube....