User Activity

Posted on November 06, 2017 at 19:19I can select this configuration in STMCWB and generate all files, but the compiler complains in line 424 of MCTasks.c  oCurrSensor[M1] = (CPWMC)IF3XX_NewObject(&PWMnCurrFdbkParamsM1, &ICS_DDParamsM1);Error[Pe167]:...
Posted on June 02, 2017 at 21:07I have several successful designs with STM32 PMSM FOC LIBv4.0, but from time to time I noticed some irregularities, causing the motor to 'click' while spinning (1kW PMSM). It sounds like someone is hitting it with a s...
Posted on March 18, 2015 at 13:42I am currently stuck with a strange phenomenon, and I am not sure anymore if what I do is how I should do it... In my appliaction with the ST FOC library 4.0, I need to do some additional A/D conversions. This needs ...
Posted on December 11, 2014 at 16:05Hi, I am trying to use the FOC4.0 library with dual rotor angle feedback, namely hall plus encoder. I can set this configuration via the GUI (I have to manually edit the generated header files because of a bug in ...
Posted on October 27, 2014 at 09:49Hi Gigi, I have a motor with rather unusual electrical parameters (low inductance, high number of poles, very high electrical rpm), and the generated output files for these settings are not usable. The compiler co...