Skip to main content
Mikk Leini
Senior
April 6, 2015
Question

Wrong Hall sensors alternate function

  • April 6, 2015
  • 2 replies
  • 584 views
Posted on April 06, 2015 at 14:55

Hi,

I'm using ST PMSM FOC 4.0 with STM32F303RB and Hall sensor. Hall sensors are on PORTC pins 6, 7 and 8. Used as TIM3 channel 1-3 inputs. Code is generated from the MC workbench. Symptom is - hall sensor signals are pulled low by the MCU. So i digged into peripheral registers with debugger and found that PC6, PC7 and PC7 have alternate function 1 which is EVENTOUT. They shoulduse AF2 which is TIM3_CHx. In library header file called SystemNDriveParams.h there's a struct which is initialized with Hall sensor alternate functions. There's also a default AF assignment:

/* TBR after final test with WB */
#if !defined(H1_GPIO_AF) 
#define H1_GPIO_AF GPIO_AF_1 
#endif 
#if !defined(H2_GPIO_AF) 
#define H2_GPIO_AF GPIO_AF_1 
#endif 
#if !defined(H3_GPIO_AF) 
#define H3_GPIO_AF GPIO_AF_1 
#endif

As the H1/H2/H3_GPIO_AF are not generated by workbench then they get the default values (AF1). Maybe the Workbench can be updated so it also generates correct alternate functions? #hall-alternate-function
This topic has been closed for replies.

2 replies

Gigi
ST Employee
April 7, 2015
Posted on April 07, 2015 at 09:23

Yes, it is someting that we already discovered in

/38f0550c

thread.

We will fix in next version.

Ciao

Gigi

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards