STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9548 Views
  • 5 replies
  • 3 kudos

steval-dpsllck1 board

I have a steval-dpsllck1 board.If I want to initialize due to a program problem in the board, if I use the Full Bridge 3 kW LLC STM32F334x V1.6.BIN file provided by ST, is it initialized for normal operation?

Kyoun.3 by Associate
  • 747 Views
  • 0 replies
  • 0 kudos

Resolved! Can the STSPIN32G4 be used to drive a brushed motor?

Hello - I'm wondering if the STSPIN32G4 can be utilized to drive a brushed motor rather than a three-phase brushless motor that it is marketed for. Alternatively, are there any chips within STMicro that are meant for brushed motors that have a combi...

How to run high voltage PMSM with STEVAL-HKI001V2 board?

Hello, I try to run PMSM motor with Steval-HKI001V2 board. Unfortunately, this board does not support motor profiler software, so I measured the motor parameters manually.I watched all the Motor Control online video courses and configured the drive p...

DJusz.1 by Associate II
  • 3344 Views
  • 4 replies
  • 0 kudos

What is the time scale in plot of ST Motor pilot?

Hi everyone! I use ST Motor pilot to control the motor. The motor reference is 354 RPM. Quantity of pole pairs is 10. Phase period must be 60 / (354 * 10) = 17 ms. But when I display the electrical phase plot, I see that the period of the phase is 1...

0693W00000QN2upQAD.png
aPott.1 by Associate II
  • 1244 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with PWM stopping after commutation event.

Hello - i'm new to STM32 MCU's (mostly have been using 8bit AVR's or OS based Raspberry Pi). I've been trying to implement a 6-step motor control (making everything from scratch as a learning experience). I picked TIM4 and TIM8 in a master-slave conf...

0693W00000QNBFJQA5.png
RobErPOL by Associate II
  • 1916 Views
  • 2 replies
  • 1 kudos

Hi. I am really battling with this cube IDE and environment. I finally managed to communicate with my STEVAL Ptool 2v1 after a great deal of fiddling around, however, i received the following, can anyone tell me what to do......

Info : accepting 'gdb' connection on tcp/3333Warn : GDB connection 2 on target STM32F031C6Tx.cpu not haltedError: timed out while waiting for target haltedError executing event gdb-flash-erase-start on target STM32F031C6Tx.cpu:TARGET: STM32F031C6Tx.c...

DDoug.2 by Associate
  • 945 Views
  • 0 replies
  • 0 kudos

Can someone tell me what T-noise and T-rise are in the Current Sensing block of the Motor Control Workbench?

I am using the IHM17M1 power board which is not supported out of the box. I have it working quite well by configuring it as a custom board. However I don't know how to set the t-rise and t-noise values. I can't find any reference to them in the docum...

SCrum.1 by Associate III
  • 9596 Views
  • 18 replies
  • 0 kudos