STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4869 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9547 Views
  • 5 replies
  • 3 kudos

Resolved! TIMER 13

Hi,I have an issue with calling Timer13 from model.cpp. For instance, htim13.Instance->CCR1 = 95. for instance fails to load. Wasn't a problem for CM7.c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-...

MCSDK error code 16 or 32

Hi, I am working on a customized board powered by STSPIN32F01B, FOC is used with 3 external OPAs for each shunt resistor. The code is generated by MCWB 5.Y.4. The SDK keeps returning error code 16 or 32 after pressing the start/stop button. I have b...

0693W00000Su23uQAB.png 0693W00000Su23pQAB.png 0693W00000Su20mQAB.png
YWang.15 by Associate II
  • 2524 Views
  • 4 replies
  • 0 kudos

Resolved! Can the evaluation board of the P-NUCLEO-IHM03 pack be used with expansion boards for controlling a stepper motor and brushed motors?

HiThere is this motor control nucleo Pack P-NUCLEO-IHM03 which includes the NUCLEO-G431RB evaluation board, the X-NUCLEO-IHM16M1 expansion board and Gimbal motor GBM2804H-100T. I cannot find further information if the included evaluation board can be...

MKron.1 by Associate
  • 1855 Views
  • 2 replies
  • 0 kudos

When will dual drive be supported by X-Cube-MCSDK 6

Dual drive support was removed from the MCSDK when version 5.Y.0 was introduced. The release notes for MCSDK V6.0.0 states:"Dual drive is no more supported at the moment. Support for this feature will be reintroduced in a future release of the SDK"Is...

MCU keeps dying at "steval-ctm010v1".

hi~We are testing the motor development kit.MCU keeps dying at "steval-ctm010v1".220V in, RS232 cable is connected.The MCU dies when the debugger is connected.The debugger connection was not possible, so I connected the C82 capacitor NRST pin to the ...

mkim.2 by Associate II
  • 1411 Views
  • 2 replies
  • 0 kudos

Resolved! Low Inductance BLDC Motor Current Signal

Hello There,I am currently work on 6 - Step (Trapezoidal) Control and have developed my software with Nucleo - F302R8. I have a low inductance(23uH) bldc motor. When I've tested this motor with my software, current signal doesn't look right. Also, we...

0693W00000NsgAcQAJ.png 0693W00000NsbHZQAZ.png