STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

Wrong code in R3_2_CurrentReadingCalibration?

used sdk : 5.4.7mcu : stm32f446redual motorIn function R3_2_CurrentReadingCalibration has below code: pHandle->PhaseAOffset >>= 3; pHandle->PhaseBOffset >>= 3; pHandle->PhaseCOffset >>= 3;But NB_CONVERSIONS is defined 16u, So is it true the right cod...

llm by Associate III
  • 1542 Views
  • 1 replies
  • 0 kudos

Resolved! problem with stspin32g4 debugging

Hello, I need help with stspin32g4 I'm programming it with nucleo-64 SWDI wrote a program with blinking led, then trying to start debbugging, i got "Break at address "0x1fff4b14" with no debug information available, or outside of program code."despit...

Tomuello by Associate II
  • 4134 Views
  • 3 replies
  • 0 kudos

problem about usage of steval-esc002v1

I succeeded in attaching steval-esc002v1 to the px4 system.However, there is a problem that the motor is not smoothly controlled through the controller. If you look at the video, it looks like it's moving by step. Can you tell me what parameters I ne...

LukeBaek by Associate
  • 1766 Views
  • 2 replies
  • 0 kudos

MotorControl reference pack not found

2023-03-25 18:35:21,503 DEBUG [Main.lambda$run$0] Arguments: [-ioc, E:\t1\6Steps-NUCLEOF401RETx-IHM07-BullRunning\6Steps-NUCLEOF401RETx-IHM07-BullRunning.ioc, -xdm, E:\t1\6Steps-NUCLEOF401RETx-IHM07-BullRunning\6Steps-NUCLEOF401RETx-IHM07-BullRunning...

wliu.2 by Associate
  • 3973 Views
  • 4 replies
  • 0 kudos

Resolved! Change max current limit during RUN state

Hello everybodyI'm using ST Motor Control 5.4.1 to drive a BLDC motor. It works fine, and I'm able to drive in SPEED MODE my motor, changing speed and with the system that can react to load changes.I would like to realize a software limit, so I can l...

Tuning the Position control

Finally was possible run the motor on my CNC machine and do a position control, I want to share the graph that I received from Current_Position register.There is some overshoot in my position control and I would like to tune it as much as possible.So...

0693W00000aIbemQAC.png
RKhal.7 by Associate
  • 1961 Views
  • 1 replies
  • 0 kudos

Resolved! Current PI sampling period for STMC FOC SDK

For calculating apriori PID parameters when running ST FOC SDK, you obviously need to consider the sampling time of the regulator for the integral term. According to UM1052, current sensing is synchronous to the PWM. Is the sampling period of the cur...

Its regarding driving of BLDC Motor

Dear Team,In a project for our client we are selected an ST solution for time saving and for reliability as per the previous interaction between us. But now we are in a great trouble and asking for your support on same.X NUCLEO IMH 07M1NUCLEO F302R8B...

KR.4 by Associate II
  • 1309 Views
  • 1 replies
  • 0 kudos