STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

Resolved! Motor only moving when quadrature encoder is rotated

I am trying to move a BLDC motor with encoder feedback in closed loop. When passing a speed/torque reference nothing happens. But when I move/rotate the encoder, the motor starts spinning according to the speed of the encoder rotating. The motor is o...

UmutU by Associate III
  • 7987 Views
  • 12 replies
  • 1 kudos

Resolved! STSPIN230 Evaluation board -> X-NUCLEO-IHM11M1

Hi,In X-NUCLEO-IHM11M1,1) What is the Formula to convert the Current feedback Output from OPAMP ?2) What is the relation of the voltage read in current Feedback pin and the motor Current value? 

NIVI_0-1693207100615.png
NIVI by Associate III
  • 1368 Views
  • 1 replies
  • 0 kudos

EVSPIN32G4 CLONE - MC_BREAK_IN Error (MC 5.Y.3)

I designed clone of EVSPIN32G4 and can't resolve issue.I generated application for EVSPIN32G4 and motor rotate without any problem, but on my PCB I have MC_BREAK_IN. Why TIMx_BRK_M1_IRQHandler() function is called?I can't find issue in my design - i...

ketchup by Associate III
  • 1244 Views
  • 1 replies
  • 0 kudos

When will ST Motor Profiler support EVSPIN32G4?

The EVSPIN32G4 is not an option when you 'select hardware' in the latest version of the Motor Profiler (5.Y.4). Will it be supported in an upcoming release? Also, is there any plan to support higher RPM profiling? The limit is 16kRPM right now.

WSega.1 by Associate II
  • 1209 Views
  • 1 replies
  • 0 kudos