STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1749 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4901 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9612 Views
  • 5 replies
  • 3 kudos

MotorControl Workbench 5.Y.4 Problems

Hi Community,I just start desiging a AC induction motor driver with motor control workbench 5.Y.4.But I have some problem about it. I can not generate code. I had try many ways but always same result. Its finished with "Comleted with errors" message....

Mnemonic_0-1706168192581.png
Mnemonic by Associate III
  • 4961 Views
  • 9 replies
  • 2 kudos

AC Servo Motor with STM32f407

Hello guys, I'm looking to control an AC Servo motor with STM32f407- Discovery kit. There are a lot of resources for DC motor, but i couldnt find many for AC Servo. Can anyone suggest on how to approach or share me some resources? Thanks in advance.

MCSDK

Hello, I am using a G030C8T6 MCU with mcsdk version 6.2.1 and the latest version of cubemx to create a motor program, but with the G0 chip library version 1.6.2 and 1.6.1, it creates the bus voltage sampling incorrectly, and it is only correct if I a...

iskan by Associate III
  • 1256 Views
  • 1 replies
  • 0 kudos

MCSDK 6.2.0 bug - Virtual V_bus_sensing

When disabling Bus Voltage Sensing and Temperature Sensing in MC WB 6.2.0 the MC Application results in HardFault. After some debugging I found that the last release of the MCSDK has made a minor change to RCM_ReadOngoingConv(). This means that when ...

Motor drive product recommendation

Hi, I have an electric assist power steering column I have been working on building a control module for. It uses a 630w IPMSM motor with hall sensors and has a supply voltage of 12-14V DC. I have managed to get the motor to run with a G431-ESC1 and ...

TRowe by Associate II
  • 1269 Views
  • 1 replies
  • 0 kudos

Resolved! trouble with B-G431-ESC1

Hi, I have been working with the B-G431-ESC1 for some time.I profiled my motor with ST Profiler and loaded the .JSON file on Workbench and generated the code.My final goal is to be able to control the speed of my motor by sending a PWM signal to the ...

Jess32 by Associate II
  • 2528 Views
  • 2 replies
  • 0 kudos