User Activity

Hi, I am figuring out how 6-step algorithm works. I generated a project using 6-step algorithm with B-G431B-ESC1.In the ADC settings, ADC1 consisted of 2 regular channel (Vbus, Temp) and 1 Injected channel (Bemf_W)So I thought ADC2 should be consiste...
Hi, I'm doing a project which sends CAN data from B-G431B-ESC1 board to sth else(NI cRio).Just to make sure, do I have to set CAN TERM Pin(PC14) high by setting it     GPIO_OUTPUT    GPIO output level : High or is it high by default?I don't understan...
Hi,I'm currently working on sending signals through FDCAN or UART of B-G431B-ESC1 while driving a motor.I have written a debug code which sends UART data when a button is pressed.However, the function is called once and never called again, nor the mo...
Hi, I am having a trouble using MCWorkbench 6.1.1When downloading a project generated from MCWorkbench demo to my B-G431B-ESC1, this happens(the rotor moves for some angle per each second while making a wierd noise. It temporarily stops when I push t...
similar question as https://community.st.com/s/question/0D53W00001wHk5BSAS/motor-wont-start-with-motor-pilotI am trying to run a BLDC motor using Motor Pilot 6.1.1 with B-G431B-ESC1.Here's my process.profile motor using motor profilergenerate code us...
Kudos given to