STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9560 Views
  • 5 replies
  • 3 kudos

About board EVSPIN32G4

Hello, I need help the product I mentioned EVSPIN32G4 I've been trying for a long time to find the pins on the board to control GPIO signals instead of SPI InterfaceI need to find these pins on the board:I/O control terminalGND Ground wireF/R Forward...

How to controll esc with pwm signal from RC controller

So i have this simple code for pwm input for the rc controller :void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef* htim){if (htim->Instance == TIM2){if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1){capture_value[0] = HAL_TIM_ReadCapturedValue(htim, TIM...

Matyáš by Associate II
  • 7062 Views
  • 8 replies
  • 0 kudos

PWM Motor Control with STM32

So, After many hours of suffering and understanding the basics of CubeIDE I got stuck and cant find any solution.My main goal was to control bldc motor by RC controller and this is what i have achieved so far :void HAL_TIM_IC_CaptureCallback(TIM_Hand...

Matyáš by Associate II
  • 8213 Views
  • 1 replies
  • 0 kudos

Resolved! Looking for ST's full code norm

Hey guys,Recently I was reading code from X-CUBE-MCSDK and was amazed at the well organised style. So I was just wondering if there is a full code specification or document for me, which would be of great importance.Apologies for my poor English and ...

DGYin by Associate
  • 2050 Views
  • 3 replies
  • 1 kudos