STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1743 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4892 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9594 Views
  • 5 replies
  • 3 kudos

Resolved! Rotary encoder for RPM calculation

Hi team,I have rotary encoder (Model - OVW2 -2048-2MC). Its resolution is 2048P/R. I get the encoder count via uart, but I have a problem, when encoder rotate continuously it does not give the data via uart, move slowly the encoder it update the valu...

Resolved! Unable to set open loop voltage

**EDIT: I misunderstood the implementation of the open loop mode, as I thought it was performing open loop SVPWM at a particular modulation index. After reviewing the open loop documentation within the motor control docs I now understand that this is...

cdoel by Associate II
  • 1887 Views
  • 1 replies
  • 0 kudos

Profiling a motor draws a huge amount of current

Hello,I have a custom inverter board which is designed for high power applications 100A+. I have individually tested the hardware functionality of the inverter and all seems to be well. However, when I run the motor profiler, a huge amount of current...

cdoel by Associate II
  • 1041 Views
  • 0 replies
  • 0 kudos

Resolved! Moto Profiler does not reach maximum engine speed.

Hi, I am using ST Motor Pilot Tool (profiler) V1.2.9.With the B-G431-ESC1 plate and the A2212/13T motor (technical sheet attached).I can't get the motor above 5200 RPM. Please note that to get to 5200 rpm I had to increase the overvoltage to 80% beca...

Motor profiler.jpg
OttoBCN by Associate II
  • 5405 Views
  • 7 replies
  • 0 kudos

Immediate Over-Current Fault in 6 Step Mode

HelloAfter trying to run a EVSPIN32F06Q2S1 in FOC Mode, which is failing at the moment (i'm working on it), i tryed to run on 6 step mode and see if this works.So i configured the board via mcwb 6.3.0, made the hardware chances which the mcwb told me...

L_e_o by Associate II
  • 1664 Views
  • 1 replies
  • 0 kudos

Resolved! Datasheet unit error on RON_OD, STSPIN32f0601

Hey all, i believe i've found a mistake on the stspin32f0601 datasheet.  https://www.st.com/en/motor-drivers/stspin32f0601.html Page 12, RON_OD, Units are in Watts instead of Ohm, I believe this is supposed to be the value of RON_OD.   Thank you  

kevinganhito_0-1717058991219.png kevinganhito_1-1717059131018.png

Error MotorControl Workbench_6.3.0 tool

Hello, I am using the MotorControl Workbench_6.3.0 tool.and it gives me an error when generating the project.In the end it tells me completed with errors.What is happening wrong?Thank you very much for your time. 

Error.jpg
OttoBCN by Associate II
  • 1664 Views
  • 2 replies
  • 0 kudos

MCSDK and USART

Hello, I have following problem:I generated a project using MC Workbench (6.3) and everything works with Motor Pilot (1.2.9). For debugging I would like to have a serial output over the same USART as the motor pilot. For start just print "Hello World...

Coolstep by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

Resolved! EVALKIT-ROBOT-1 Example code build error question

I purchased EVLAKIT-ROBOT-1 and am trying to run it.I request information for operation.An error occurs when building the example code.I wonder if the problem is caused by the software tool version. If so what version of software should I run it with...

kimsdo by Associate
  • 1210 Views
  • 1 replies
  • 0 kudos