STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1610 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4759 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9486 Views
  • 5 replies
  • 3 kudos

Immediate Over-Current Fault in 6 Step Mode

HelloAfter trying to run a EVSPIN32F06Q2S1 in FOC Mode, which is failing at the moment (i'm working on it), i tryed to run on 6 step mode and see if this works.So i configured the board via mcwb 6.3.0, made the hardware chances which the mcwb told me...

L_e_o by Associate II
  • 1621 Views
  • 1 replies
  • 0 kudos

Resolved! Datasheet unit error on RON_OD, STSPIN32f0601

Hey all, i believe i've found a mistake on the stspin32f0601 datasheet.  https://www.st.com/en/motor-drivers/stspin32f0601.html Page 12, RON_OD, Units are in Watts instead of Ohm, I believe this is supposed to be the value of RON_OD.   Thank you  

kevinganhito_0-1717058991219.png kevinganhito_1-1717059131018.png

Error MotorControl Workbench_6.3.0 tool

Hello, I am using the MotorControl Workbench_6.3.0 tool.and it gives me an error when generating the project.In the end it tells me completed with errors.What is happening wrong?Thank you very much for your time. 

Error.jpg
OttoBCN by Associate II
  • 1611 Views
  • 2 replies
  • 0 kudos

MCSDK and USART

Hello, I have following problem:I generated a project using MC Workbench (6.3) and everything works with Motor Pilot (1.2.9). For debugging I would like to have a serial output over the same USART as the motor pilot. For start just print "Hello World...

Coolstep by Associate
  • 849 Views
  • 0 replies
  • 0 kudos

Resolved! EVALKIT-ROBOT-1 Example code build error question

I purchased EVLAKIT-ROBOT-1 and am trying to run it.I request information for operation.An error occurs when building the example code.I wonder if the problem is caused by the software tool version. If so what version of software should I run it with...

kimsdo by Associate
  • 1174 Views
  • 1 replies
  • 0 kudos

IHM03A1 with Nucleo stm32F401 Speed issue

So i've been having an issue with the Powerstep01 driver to run some stepper motors. In my application i'm running 4 stepper motors with a wide speed range (up to 850 RPM or 2980 steps/s). These motors are STP-MTRH-24079D which have parameters (Iph =...

bkeating by Associate
  • 1624 Views
  • 1 replies
  • 0 kudos

STSPIn32F0601 based ACIM motor Control

Hello,we have STSPIN32F0601 based custom designed board for PMSM motor Controller. we have generated FOC code using  MC workbench and it works ok.Now we want to use ACIM motor in this Hardware (with Little change or No change in Hardware). we are una...

PPate.2 by Associate III
  • 1411 Views
  • 2 replies
  • 0 kudos

Evspin32G4-Dual Tuning Speed Control

 Hello everyone,I am currently working on a project involving an Evspin32G4-Dual Board, equipped with two brushless motors (Hover Board motors 36V-10A-500 rpm-Hall Sensors).I have completed profiling the motors and their hall sensors using MC Workben...

ItzSam by Associate II
  • 1488 Views
  • 1 replies
  • 0 kudos

Resolved! MCWB 5.4.3 Encoder Position Problem

I use 2048 PPR encoder for speed control. It work well.But if I change the motor mode from speed to position control,something goes wrong.If we select Z signal for shaft zero alignment,the code after reset belowMC_StartMotor1();while (MC_GetAlignment...

0693W000003Q5fcQAC.jpg
LSHEN.1 by Associate II
  • 2399 Views
  • 4 replies
  • 0 kudos