STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL fails to compile

Hi,MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL fails to compile with the errors below: C:/Users/Ian/.st_workbench/projects/MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL/Src/mc_tasks.c: In function 'MC_RunMotorControlTasks':C:/Users/Ian/.st_workbench/projects/MCSDK-PKG00...

murpia by Associate II
  • 1140 Views
  • 1 replies
  • 0 kudos

Resolved! Questions on roadmap for ACIM supoport

Hello,I am considering transitioning to the ST MCU family for my inverter projects. The primary type of motor I use is ACIM. From what I have read, the latest version of the MCSDK/MotorControl Workbench only supports ACIM through two examples, and it...

Paiva404 by Associate
  • 2257 Views
  • 2 replies
  • 0 kudos

Tutorial -STEVAL-SPIN3202/STEVAL-SPIN3204

Hello Team,   we try to run the motor using motor control work bench, STM mx and STM cube IDE. motor run for 3 to 5 sec and stop.Is there any tutorial or any document or example we can follow step by step and understand each parameter related to STEV...

Sayali23 by Associate II
  • 1221 Views
  • 1 replies
  • 0 kudos

Where does G431 TIM1 ITR1 acturlly from?

Hello everyone! I use a BLDC with hall sensors drivered by ST's B-G431B-ESC1 inverter board, and demo code generated by MC Workbench. Use ST Motor pilot V1.2.5 - MC_FOC_SDK have a test, BLDC is runing and everything is ok. In the demo code, TIM4 use ...

xiepan_1-1715054384150.png xiepan_2-1715054420279.png
xiepan by Associate
  • 1477 Views
  • 1 replies
  • 0 kudos

Motor Control Help - EVLDRIVE101-HPD

Hi,I can't manage to get my motor to work with the EVLDRIVE101-HPD board. I have generated the FOC firmware and uploaded it to the board through STM32CubeIDE. See attached for main.cIs there something else I need to do? I have followed everything in ...

mitch1 by Associate II
  • 7573 Views
  • 10 replies
  • 0 kudos

Why the start of ovm mode is set to these value?

#define OVM_VREF_MODE1_START ((int32_t)29717) #define OVM_VREF_MODE2_START ((int32_t)31186)The ratio between these two value is not sqrt(3)/2. What is the voltage unit used in these calculation? Or when a have a Valpha equal to 32767, what is the tru...

Konecho by Associate II
  • 1301 Views
  • 2 replies
  • 0 kudos