User Activity

Can someone help me understand the profile of the trapezoidal move? for example if I would like to make a movement of 10 radiance in 10 seconds using the MC_ProgramPositionCommandMotor1 how much of the 10 seconds will be acceleration, constant veloci...
Hi, NUCLEO-G431RB + X-NUCLEO-IHM07M1MCWB 5.Y.3 + STM32CubeIDE 1.7.0Maxon motor combination: 200142 + 166935 + 673026BLDC motors are supposed to be "silent" however this doesn't seem to be the case when I attempt to drive the motor with the combinatio...
NUCLEO-G431RB + X-NUCLEO-IHM07M1MCWB 5.Y.3 + STM32CubeIDE 1.7.0Maxon motor combination: 200142 + 166935 + 673026I have created a project to drive a BLDC motor with the above mentioned equipment, I was able to create a basic project to drive the ...
Hardware: NUCLEO-F303RE + X-NUCLEO-IHM07M1Software: MCWB 5.Y.3 + STM32CubeIde 1.7.0Motor combination: 200142 + 166935 + 673026 (12V + 21:1 + 1024CPT) Project requirements: minimum speed: 0.4 RPM max speed: 3000 RPM (motor speeds NOT gearbox o...
I have created a position control project using the followings. Nucleo-F302R8IHM07M1MotorControl Workbench 5.Y.1STM32CubeMX 6.1.0After creating a basic project I have set up a timer generating an interrupt every 1ms. In the interrupt handler I have p...
Kudos from