Hello everyone.I am using the Motor Control WorkBench 6.3.0 application to generate the project. The inverter board isB-G431B-ESC1. The motor is a 2-pole BLDC, 8.5V, it has a very low inductance of 0.04mH, an Rs of 0.37ohms and the B-Emf constant is ...