STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1725 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4873 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9558 Views
  • 5 replies
  • 3 kudos

Port Open and try to configure the board

Motor Control Workbench v6.3.0I made a clone of the EVSPING4-ACT board but I'm not able to connect the Motor Pilot to it.  I'm using the same firmware, same debugger, and same power supply.  I confirmed the pin connections are correct and it looks li...

Errors and Baudrate in MCSDK

I connected the B-G431-ESC inverter to a DJI2312 motor and created the project on MC Workbench version 6.1.0 (I also tried 6.1.3).I would like to use the motor pilot but when I press on "discover board" the board is not recognized.In the generated th...

luke514_0-1728571874546.png
luke514 by Senior
  • 778 Views
  • 0 replies
  • 0 kudos

MCSDK 6.3.1 release?

Hello there,I am trying to generate 6 Step motor control firmware for some custom hardware based on the B-G431B-ESC1.I would like to use the ESC PWM input feature, however the auto-generated code throws errors. This feature works fine in FOC mode, an...

Resolved! MC SDK documentation for data packet structure?

Hi,I am trying to understand the protocol, especially how to interpret the data packets to have custom code for auto motor ramp-up.I see there are some documents under MC workbench -> About. However, I still cannot find the details about the data pac...

MC Observer + Cordic

I am trying to operate an 8-pole pair 48V PMSM motor withSTEVAL-CTM009V1IHM09M2Nucleo-G431RBSensorless with Observer + Cordic. I have run a motor profile with EVALSTDRIVE101. I have entered the parameters for the motor in MC Workbench 6.3.1. I have s...

ktim by Associate II
  • 2147 Views
  • 3 replies
  • 0 kudos

PWM highlight Timer

Hello, I am new in STM32Cube. I try some test with PWM timer 4. It  works. I see the signal on oscilloscope. But why is not in clock configuration  highlighted the timer clock and I can not also change the clock source.Best regards.  

Scipio_0-1728316741615.png Scipio_1-1728316770363.png
Scipio by Associate
  • 933 Views
  • 1 replies
  • 0 kudos